termination resistor of DRAM_SDCLK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

termination resistor of DRAM_SDCLK

ソリューションへジャンプ
964件の閲覧回数
renefed
Contributor I

Hello,

I have a question about the termination resistor of DRAM_SDCLK in the i.MX6UL reference design (MCIMX6UL-CM).

Why is R206 dimensioned with 470R? Most guidelines recommend about 200R.

R206.JPG

Many thanks in advance.

Regards

René

ラベル(1)
0 件の賞賛
返信
1 解決策
737件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi René

you are right recommend value is about 200R, but for reducing power consumption

was used 470R which also worked fine.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
738件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi René

you are right recommend value is about 200R, but for reducing power consumption

was used 470R which also worked fine.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------