temperature sensor pct2075 linux driver for imx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

temperature sensor pct2075 linux driver for imx6

2,807 Views
letan
Contributor III

Hello all,

I am working on our custom project that uses the PCT2075 as temperature sensor. But I can NOT find this driver on the latest imx6 BSP.

Could you all please help me on this?

I am looking forward to your respond!

Thanks,

Tan

Labels (5)
0 Kudos
Reply
1 Reply

2,154 Views
art
NXP Employee
NXP Employee

There is no dedicated driver for the PCT2075 temperature sensor in the i.MX6 series Linux BSP. You can operate this sensor using existing general I2C driver, already included into the BSP, please refer to the Chapter 36 of the attached document.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------