support wi-fi module

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

support wi-fi module

1,755 Views
sachusanal
Contributor III

Hi sir ,

I have IMX6Q sabresd board Evaluation kit with me(which is purchased from freescale) let me know this board support wi-fi module? i didnt find any wi-fi connector in this device. so i think shall i connect the USB wi-fi dongle on Microusb otg port with help micro usb connector.the  demo image have support wi-fi  module or not

Labels (1)
0 Kudos
Reply
3 Replies

1,681 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
Reply

1,681 Views
saurabh206
Senior Contributor III

Hi

Which board you have purchase?

If you have purchased SABREAuto board than SDCard interface is available

SABRE|Automotive-Infotainment|i.MX6|Freescale

Thanks

Saurabh

0 Kudos
Reply

1,681 Views
sachusanal
Contributor III

Hi Sourabh,

I am using sabresd board

0 Kudos
Reply