support wi-fi module

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

support wi-fi module

1,756件の閲覧回数
sachusanal
Contributor III

Hi sir ,

I have IMX6Q sabresd board Evaluation kit with me(which is purchased from freescale) let me know this board support wi-fi module? i didnt find any wi-fi connector in this device. so i think shall i connect the USB wi-fi dongle on Microusb otg port with help micro usb connector.the  demo image have support wi-fi  module or not

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,682件の閲覧回数
igorpadykov
NXP Employee
NXP Employee
0 件の賞賛
返信

1,682件の閲覧回数
saurabh206
Senior Contributor III

Hi

Which board you have purchase?

If you have purchased SABREAuto board than SDCard interface is available

SABRE|Automotive-Infotainment|i.MX6|Freescale

Thanks

Saurabh

0 件の賞賛
返信

1,682件の閲覧回数
sachusanal
Contributor III

Hi Sourabh,

I am using sabresd board

0 件の賞賛
返信