stuck at starting kernel

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

stuck at starting kernel

18,564件の閲覧回数
srinivas_123
Contributor III

i am using imx8mplus lpddr4 evk. and i build the yocto 6.1.55 BSP version

for custom board i changed the DRAM size to 1GB , and frequency to 2400MTS.

After booting up , it stuck at Starting Kernel . if anyone know why this is happening. where i did the mistake  . please help me out.i attached boot log.

 

Regards ,

Srinivas

0 件の賞賛
返信
2 返答(返信)

18,545件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Apparently you don't have enough memory to boot the MX8MPlus, we suggest at least 2GB of RAM.

Regards

0 件の賞賛
返信

18,524件の閲覧回数
srinivas_123
Contributor III

@Bio_TICFSL 

Thank you for your response. just confirm, I have read a few NXP forums. they suggest disabling some nodes(which are not required). so, I disabled HDMI, pCIe, and LVDS. after that, it moves ahead. and again kernel gets stuck and shows panic.

am I following the correct way or not?

I observed the SP/PC alignment exception in the log. Does this issue come because of less size of the memory.?

I have attached a log file. please check once.

0 件の賞賛
返信