splashscreen on android os

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

splashscreen on android os

3,225件の閲覧回数
sachusanal
Contributor III

Dear Sir,

I am using Android lolipop source for  IMX6qsabresdp board .

I build the images by using user guide .

I need to set my custom splash screen on android booting.

now my image shows boot loader loading time free scale semiconductor then shows kernel tux then shows android at the time of kernel and file system booting.

could you please help me to change these three images and load my  custom splash image please help me.

Regards

Sachu

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

3,029件の閲覧回数
sachusanal
Contributor III

Hello sir ,

could you please help me to set splash image on lolipop board.

from where i can store my spalsh screen image

0 件の賞賛
返信

3,028件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

also it may be useful to look at attached  L5.0

Android_User's_Guide.pdf p.23.

Best regards

igor

0 件の賞賛
返信

3,028件の閲覧回数
sachusanal
Contributor III

Dear Igor ,

Could u please help me to edit the boot image , which file i can edit for image changes.

its an urgent task , please help me

0 件の賞賛
返信

3,028件の閲覧回数
saurabh206
Senior Contributor III
0 件の賞賛
返信