sources/poky/meta/recipes-kernel/perf/perf.bb:do_compile) failed with exit code '1'

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

sources/poky/meta/recipes-kernel/perf/perf.bb:do_compile) failed with exit code '1'

668件の閲覧回数
Embedded-world
Contributor IV

Dear Experts,

I'm currently working on the BSP images for an i.MX6ULL processor-based custom embedded board. I have created the machine file for the respective board, & I'm trying to create a QT6 feature image. For this, I used the following configuration and executed the command:

 

DISTRO=fslc-xwayland MACHINE=imx6ull-versa256 source calixto-setup-release.sh -b build-xwayland

$bitbake imx-image-full"

 

But, I encountered the following issue:

Output:
ERROR: Task (/home/calixto_admin/calixto-yocto-bsp/sources/poky/meta/recipes-kernel/perf/perf.bb:do_compile) failed with exit code '1'

Could someone please help me resolve this issue?


Regards,
Ravikumar

0 件の賞賛
返信
1 返信

642件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

Please check the failure log 

Best Regards
Zhiming

0 件の賞賛
返信