setting application at the starting time

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

setting application at the starting time

1,185件の閲覧回数
sachusanal
Contributor III

Hi Sir,

I am using IMX6qsabres board for android lolipop image flashing.

i built android lolipop image by using Android users Guide.

I need to run my application at the starting time , intsed of loading desktop.

From which file i can include my application for running at the starting time

ラベル(1)
0 件の賞賛
返信
1 返信

1,133件の閲覧回数
art
NXP Employee
NXP Employee

First, look here for some "hardcoded" solution:

http://stackoverflow.com/questions/6391902/how-to-start-an-application-on-startup

Then, there are some ready to use launcher applications in Google Play Market, for example, the following one:

https://play.google.com/store/apps/details?id=com.autostart


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信