set read bl len failed !

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

set read bl len failed !

Jump to solution
1,362 Views
Xavier
Contributor III

I am developing a card based on i.MX535 processor. All seem good, but I encountered a problem with µSD on slot SD1. When U-boot tries to load Linux kernel image from the µSD to DDR, we have the message "set read bl len failed".

I tried to rescan the µSD (mmc rescan 0), but it fails.

Any idea ?


Labels (2)
0 Kudos
Reply
1 Solution
1,131 Views
imxcommunitysco
Senior Contributor II

Are you able to see some clock signal comming out from SD interface after the mmc rescan command?. You could use a scope for this.

Try to use another device number on the SD.

View solution in original post

0 Kudos
Reply
1 Reply
1,132 Views
imxcommunitysco
Senior Contributor II

Are you able to see some clock signal comming out from SD interface after the mmc rescan command?. You could use a scope for this.

Try to use another device number on the SD.

0 Kudos
Reply