sdpv write -f flash.bin -skipspl

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

sdpv write -f flash.bin -skipspl

2,719 Views
antonio_santagi
Contributor IV

Hello, I am using uuu to write to eMMC on imx8MM evk.

It works but I haven't understood what the -skipspl does when I run the command

uuu -b emmc flash.bin

it executes sdpv write -f flash.bin -skipspl.

my flash.bin file is an aggreagate of spl and u-boot, together with all the other ATF, DDR4 training and IVT .

Why the uuu emmc script adds this -skipspl that sounds like "skip programming spl" ? I couldn't find a reference about this SDPV and this option .

Thank you

0 Kudos
Reply
1 Reply

2,610 Views
igorpadykov
NXP Employee
NXP Employee

Hi Antonio

seems skipspl "skips some data when using spl" while searching uboot position

it is used by SDPV which is upgrade version of SDPU :

Support -skipspl option at sdp protocol (a4bbea24) · Commits · Librem5 / mfgtools · GitLab 

https://github.com/NXPmicro/mfgtools/releases/download/uuu_1.3.154/UUU.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply