sd2 pins in uboot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,948件の閲覧回数
michaelcarrier
Contributor III

We have a custom design that is based largely on the ul6_evk. The hardware folks decided to move the boot device from SD2 (the EVK's boot device) to sd1. u-boot can no longer boot into the kernel as expected. I know I am going to have to change u-boots IOMUX pin settings to enable sd1 but for the life of me can't figure out where those changed need to occur. We are using Yocto to do the builds and as such I believe uboot source is at <basedir>/tmp/work/imx6ulevk-poky-linux-gnueabi/u-boot-imx/2015.04-r0/git.

Any help would be greatly appreciated.

ラベル(1)
0 件の賞賛
返信
1 解決策
4,652件の閲覧回数
michaelcarrier
Contributor III

Ok, found the location and made the necessary changes to the imx6ul IOMUX. u-boot is loaded  and can load zImage and the device tree blob. The kernel is now hanging which I am sure is do to the SD card change. Anyone have a clue as to where in menuconfig I can change change the rootfs location?

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
4,652件の閲覧回数
kyle2
Contributor I

michaelcarrier‌ Can you tell us which files you changed? We are experiencing the exact same problem.

0 件の賞賛
返信
4,653件の閲覧回数
michaelcarrier
Contributor III

Ok, found the location and made the necessary changes to the imx6ul IOMUX. u-boot is loaded  and can load zImage and the device tree blob. The kernel is now hanging which I am sure is do to the SD card change. Anyone have a clue as to where in menuconfig I can change change the rootfs location?

0 件の賞賛
返信
4,652件の閲覧回数
gbiradar
Contributor IV

check out this path -> arch/arm/include/asm/<respective architecture>/<your arch_pins.h>

0 件の賞賛
返信
4,647件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

I attach the BSP porting guide for your information. You can read the Chapter 2 and Chapter 4 for more details about IOMUX and SDHC porting.

0 件の賞賛
返信
4,647件の閲覧回数
michaelcarrier
Contributor III

I have this guide and I understand the IOMUX and pin configurations. The problem I am having is where in the u-boot file structure are the changes to be made.

0 件の賞賛
返信