screen compatible for i.MX 1170 evaluation kit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

screen compatible for i.MX 1170 evaluation kit

1,099 Views
fcote
Contributor I

hi, i work on a project with the I.Mx RT 1170 Evaluation Kit and the 5.5 LCD panel RK055HDMIPI4MA0, but i want to use an other lcd, like an 7 inch screen. so can you tell me if I can plug an other one and if i can change the pinout of the MIPI interface?

Thanks

0 Kudos
Reply
1 Reply

1,084 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @fcote,

As long as the new LCD supports the MIPI interface, you should be able to use it with the RT1170 without any issues. Here's an application note that describes this interface in more detail: https://www.nxp.com/docs/en/application-note/AN12940.pdf

BR,
Edwin.