scale up a picture

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

scale up a picture

1,985件の閲覧回数
jony_oy
Contributor I

we use i.mx6 solo platform.encode in transmiting terminal,and then decode in receving terminal.using h.264

when the receving solution is 1280*720.we want to scale up to 1920*1080.however when we scale up ,we

find that the picture is out of size however we adjust it.

タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,825件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

IC module can resize and color conversion, but I don’t think IC can change the frame rate.
please check https://community.freescale.com/docs/DOC-95595


Have a great day,

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,825件の閲覧回数
jony_oy
Contributor I


we did not change the frame rate.just resize the picture.when we scale up a picture the picture will out of size the screen.

we check the source code ,when the resolution bigger than 1024. it will set two parts stripe.left and right.does any bug in

ipu in the kernel. we did not have the answer, and ask for help 

0 件の賞賛
返信