salve-spi ss Interrupt

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

salve-spi ss Interrupt

2,283 次查看
leihe
Contributor I

            hello,I have a problem,I need Interrupt signal to tell me when the data  transmission is complete ,my machine is a slave spi device,so master control when the transmission is over,I want's to check chip select Interrupt,I can't find it,is it exists in imx6D?

thank you!

标签 (4)
标记 (2)
0 项奖励
回复
3 回复数

2,137 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi lei he,

You can look at chapters 21.4.6 Interrupts and 21.7.5 Interrupt Control Register (ECSPIx_INTREG) in IMX6D Reference Manual


Regards,
Carlos
NXP Technical Support

0 项奖励
回复

2,137 次查看
leihe
Contributor I

thankyou

0 项奖励
回复

2,137 次查看
leihe
Contributor I

if i set the bit of sion,can I use gpio interrupt?

0 项奖励
回复