salve-spi ss Interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

salve-spi ss Interrupt

2,260 Views
leihe
Contributor I

            hello,I have a problem,I need Interrupt signal to tell me when the data  transmission is complete ,my machine is a slave spi device,so master control when the transmission is over,I want's to check chip select Interrupt,I can't find it,is it exists in imx6D?

thank you!

Labels (4)
Tags (2)
0 Kudos
Reply
3 Replies

2,114 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi lei he,

You can look at chapters 21.4.6 Interrupts and 21.7.5 Interrupt Control Register (ECSPIx_INTREG) in IMX6D Reference Manual


Regards,
Carlos
NXP Technical Support

0 Kudos
Reply

2,114 Views
leihe
Contributor I

thankyou

0 Kudos
Reply

2,114 Views
leihe
Contributor I

if i set the bit of sion,can I use gpio interrupt?

0 Kudos
Reply