rpmsg problem on imx6sx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

rpmsg problem on imx6sx

4,215件の閲覧回数
jingyangxie
Contributor V

Hi,all

     I have a imx6sxsabresd motherboard, when I follow the "i.MX Linux Reference Manual", loading Linux terminal imx_rpmsg_tty.ko, M4 serial port will be garbled, while without doing rpmsg communication, M4 serial port work well . Any suggestions?

PS: Linux BSP 3.14.52

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

3,936件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi jingyang

please try with "uart_from_osc" kernel boot parameter described in

Table 11. Common kernel boot parameters attached Linux Manual.

Also one can try with L3.14.52 demo images:

https://www.nxp.com/webapp/Download?colCode=L3.14.52_1.1.0_iMX6SX&appType=license&location=null 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,936件の閲覧回数
jingyangxie
Contributor V

Hi,igor

   I have added "uart_from_osc" in uboot env,M4 serial port work fine in other demos without rpmsg

0 件の賞賛
返信

3,936件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi jingyang

please check testing description in attached Linux Manual sect.

52.5 Running i.MX RPMsg Test Programs:

Run the following command and ensure that the RPMsg TTY receiving program
is running at backend when starting RPMsg TTY tests.
/unit_tests/mxc_mcc_tty_test.out /dev/ttyRPMSG 115200 R 100 1000 &

Best regards
igor

0 件の賞賛
返信

3,936件の閲覧回数
jingyangxie
Contributor V

Hi,igor

    I have followed the Manual for mxc_mcc_tty_test,but problem remains.It's normal to start running on the M4 program, but when I enter "insmod imx_rpmsg_tty.ko" at the A9 side, the serial port of the M4  will be messed up.

pastedImage_1.png

0 件の賞賛
返信