rootfs with vivante support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

rootfs with vivante support

2,670件の閲覧回数
srinivasaporam
Contributor II

Hi,

We have got imx6Q reference board for which we have cross compiled kernel.

We are able to boot to ubuntu with this board but X is giving error that not able to load 'vivante'.

We are using ubuntu-core-14.04.02-core.armhf.tar.gz (rootfs). When we are checking for vivante.so in (./usr/lib/ or ./usr/lib/xorg etc..) vivante driver support files are not there. How to get rootfs which has got vivante support or how i can make this rootfs to have vivante????

ラベル(3)
0 件の賞賛
返信
2 返答(返信)

1,879件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Srinivasa

vivante drivers are : gpu-viv-bin-mx6q-xx, xserver-xorg-video-imx-viv-xx

http://downloads.yoctoproject.org/mirror/sources/kernel-module-imx-gpu-viv-5.0.11.p7.1.tar.gz

http://downloads.yoctoproject.org/mirror/sources/xserver-xorg-video-imx-viv-5.0.11.p7.1.tar.gz

https://community.freescale.com/thread/327339

https://community.freescale.com/thread/376320

http://downloads.yoctoproject.org/mirror/sources/

http://patches.openembedded.org/patch/104949/

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,879件の閲覧回数
srinivasaporam
Contributor II

Hi Igor,

Can you please explain me how to build these and deploy to the target machine.

We already cross-compiled 3.10.53 or 3.14.14 and board is booting to ubuntu14.04. Now from above links i have got

1.kernel-module-imx-gpu-viv-5.0.11.p7.1.tar.gz

2. xserver-xorg-video-imx-viv-5.0.11.p7.1.tar.gz

is there any document that explains installing above ?????

0 件の賞賛
返信