rgmii loopback test for imx6q

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

rgmii loopback test for imx6q

1,669 次查看
pravverma
Contributor III

Hi,

We are using i.xm6q based custom board.

We are facing packet loss for size 1k+ consistently.

To debug the issue & verify the driver, I want to enable the loopback as mention in following.

Receive Control Register (ENET_RCR)[LOOP] = 1

But this bit is explained as MII internal loopback, To enable loopback we have to set MII_MODE set to 1 & RMII_MODE set to 0.

Could we use this loopback to test the RGMII driver also?

If not how to test the loopback for RGMII?

Thanks,

Praveen

标签 (2)
0 项奖励
回复
1 回复

1,479 次查看
b36401
NXP Employee
NXP Employee

Internal MII loopback described in this register supposes only MII not RGMII.

I mean we have only MII loopback in i.MX6Q processor.

Sorry for the inconvenience.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复