regmap() using a 3.10.17 kernel?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

regmap() using a 3.10.17 kernel?

ソリューションへジャンプ
2,752件の閲覧回数
johngriswold
Contributor II

Our product is built on a 3.10.17 kernel. I'm trying to incorporate support for the power-off interrupt using snvs_pwrkey.c driver. This driver was written toward a newer (4.x) kernel using regmap() and other related calls.

Am I on a fool's errand trying to get this driver working on a 3.10 kernel? Right now I'm getting a kernel panic, I think related to the return value from regmap(), in regmap_update_bits

[    1.504251] snvs_pwrkey 20cc038.snvs-poweroff: Probing...

[    1.509717] snvs_pwrkey 20cc038.snvs-poweroff: pdata maps to DC353A90

[    1.516191] snvs_pwrkey 20cc038.snvs-poweroff: pdata->snvs maps to FFFFFDFB

[    1.531681] snvs_pwrkey 20cc038.snvs-poweroff: Wakeup OK...

[    1.537285] snvs_pwrkey 20cc038.snvs-poweroff: IRQ OK...

call to regmap_update_bits (  FFFFFDFB 00000038 00000020 00000020)

[    1.542635] snvs_pwrkey 20cc038.snvs-poweroff: FFFFFDFB 00000038 00000020 00000020

[    1.550246] Unable to handle kernel paging request at virtual address fffffe1b

[    1.557494] pgd = c0004000

[    1.560239] [fffffe1b] *pgd=3f77e821, *pte=00000000, *ppte=00000000

[    1.566646] Internal error: Oops: 17 [#1] SMP ARM

[    1.571376] Modules linked in:

[    1.574497] CPU: 1 PID: 1 Comm: swapper/0 Not tainted 3.10.17-ts-armv7lts2 #12

[    1.581749] task: dc08c000 ti: dc08a000 task.ti: dc08a000

[    1.587192] PC is at regmap_update_bits+0x20/0x64

[    1.591935] LR is at imx_snvs_pwrkey_probe+0x14c/0x398

[    1.597103] pc : [<c034163c>]    lr : [<c03fcf70>]    psr: 60000113

[    1.597103] sp : dc08bd98  ip : dc08bdc8  fp : dc08bdc4

[    1.608605] r10: c0821e9c  r9 : c080b780  r8 : 00000020

[    1.613855] r7 : 00000038  r6 : 00000020  r5 : 00000020  r4 : fffffdfb

[    1.620407] r3 : 00000020  r2 : 00000020  r1 : 00000038  r0 : fffffdfb

[    1.626962] Flags: nZCv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment kernel

[    1.634297] Control: 10c5387d  Table: 1000404a  DAC: 00000015

[    1.640068] Process swapper/0 (pid: 1, stack limit = 0xdc08a238)

[    1.646101] Stack: (0xdc08bd98 to 0xdc08c000)

I'm trying to get back into Linux drivers from the relative Stone Age of 2.06. Yes, I should have just stayed immersed...:)
Thanks,

John

1 解決策
2,586件の閲覧回数
johngriswold
Contributor II

I withdraw the question. Brain death occurred at 0812 on January 18. FFFFFDFB is error code -EPROBE_DEFER.

Thanks to those who viewed my question, shook their heads, and silently walked away...

元の投稿で解決策を見る

3 返答(返信)
2,587件の閲覧回数
johngriswold
Contributor II

I withdraw the question. Brain death occurred at 0812 on January 18. FFFFFDFB is error code -EPROBE_DEFER.

Thanks to those who viewed my question, shook their heads, and silently walked away...

2,586件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Sorry to hear that!! :smileysad:.

0 件の賞賛
返信
2,586件の閲覧回数
johngriswold
Contributor II

Thanks. Yeah, I just got stupid and lazy :smileyhappy:

0 件の賞賛
返信