register value for PLL clock 999MHz

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

register value for PLL clock 999MHz

ソリューションへジャンプ
2,945件の閲覧回数
ludovicleau-mer
Contributor III

Hi,

a try to get the clock signal from a custom mipi camera board on a sabrelite board. And i have found several code for PLL clock from :

ラベル(1)
1 解決策
2,644件の閲覧回数
ludovicleau-mer
Contributor III

Ok i found the problem :

The camera was started before the init of my module. So i change it and i set the register value 0x3a ( for  999MHz) and i received the statut 3F0 for 4 lane.

I think all is ok. Now i must be check the clock  setting hsp_clk and pixel_clk.

元の投稿で解決策を見る

3 返答(返信)
2,644件の閲覧回数
ludovicleau-mer
Contributor III

I had trying all register value between 0x00 and 0xFF for the PLL clock (mipi_csi2_write(info, 0x000000XY, CSI2_PHY_TST_CTRL1);) and for each i receive several 0x200 and finally the PHY_STATE 0x2f0.

I think i have an error in my driver. Perhaps i forgot to enable something.

The clock signal was checked in the mipi before imx6 : all is ok.

Anybody have an idea on what can be the problem ?

thanks.

0 件の賞賛
返信
2,645件の閲覧回数
ludovicleau-mer
Contributor III

Ok i found the problem :

The camera was started before the init of my module. So i change it and i set the register value 0x3a ( for  999MHz) and i received the statut 3F0 for 4 lane.

I think all is ok. Now i must be check the clock  setting hsp_clk and pixel_clk.

2,644件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Thank you for posting your findings! I'm sure they'll help other community users!

0 件の賞賛
返信