"boot kernel with command debug_uart2"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

"boot kernel with command debug_uart2"

1,954件の閲覧回数
xlin
Contributor III

Hi,

On the page 12 of AN4580(which is attached herewith),  there are some steps to put  the Sololite into system idle mode under the section 5.2.4.

What does  "boot kernel with command debug_uart2" mean?

Best Regards,

Xinsi Lin

ラベル(3)
0 件の賞賛
返信
1 返信

1,862件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

The wording seems confusing but it’s most likely referring to setting up the serial console to run the steps that follow on the document. This is similar to the setup from the other i.MX6 Power Measurement App Notes.

0 件の賞賛
返信