question for i.mx6 IPU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

question for i.mx6 IPU

1,305件の閲覧回数
dingyanhong
Contributor I

we are porting RTOS system for imx6 platform and have an issue for IPU function.

Is that possible to change the parameter (such as width/height/u offset etc.) for CPMEM channel buffer without closing the channel?

We need to do Seamless switch for different resolution movies,it is more simple if the bg channel can output different resolution image (like from 720p to 1080p) without close the bg channel.

Or do you have any other proposal for this kind of function?

thanks!

ラベル(5)
0 件の賞賛
返信
1 返信

1,107件の閲覧回数
Yuri
NXP Employee
NXP Employee

According to Table 37-41 (Internal Memories Access Support and Limitations)

of the i.MX6 DQ Reference Manual regardin CPMEM : "IDMAC channel parameters

must not be changed in the CPM when the corresponding DMA channel is enabled

excluding the base addresses (EBA0 and EBA1)."

0 件の賞賛
返信