question for /dev/fb0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

question for /dev/fb0

2,460件の閲覧回数
guojunqiang
Contributor II

Dears,

Could you please tell that whether the func cfb_imageblit(...) in file cfbimgblt.c used for ?

I am porting lcdc on IMX7D,I just want to know if function  cfb_imageblit is needed when open /dev/fb0 to flush image in userspace test code.

Thank you.

ラベル(1)
0 件の賞賛
返信
1 返信

2,366件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi keil

what bsp used in the case and driver source. Just

for reference one can look at driver descriptions in attached Linux Manual

sect.6.3.4 ELCDIF Frame Buffer, sect.6.4.5 Electrophoretic Display Controller (EPDC) Interface

Linux L4.14.78_1.0.0    link
https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_4.14.78_1.0.0_ga


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信