question about pcie

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

question about pcie

2,053 次查看
ainolike
Contributor III

I'm testing PCIe with SABRE lite board. there are some questions about PCIe.

a) In chapter memory map of IMX6DQRM, it assigns a range of address as follows.

     Start address     End address     Size          Description

     01FF_C000        01FF_FFFF      16KB        PCIe register

     0100_0000         01FF_BFFF      16368KB  PCIe

I want to know the usage of the 16368KB space. Is PCIe BAR must mapped to this memory space? And is the size of BAR space must less than 16368KB?

b) I have had my board work in RC mode. How can I set PCIe working in EP mode?

标签 (6)
0 项奖励
回复
2 回复数

1,795 次查看
Yuri
NXP Employee
NXP Employee

Hello,

as for PCIe EP mode - perhaps the following helps.

Configuring the kernel for RC/EP communication

Regards,

Yuri.

0 项奖励
回复

1,792 次查看
art
NXP Employee
NXP Employee

a) Please refer to the Chapter 40 of the attached document.

b) There is no EP functionality implementation in the current Linux BSP driver.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复