pxp support needed in imx7 android.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

pxp support needed in imx7 android.

2,686 Views
sankarsalla
Contributor II

Hi All,

I am working on Imx7 android project.

It is working without pxp support,because of that my android is working very slow (it takes cpu usage above 30%).

Can i use  pxp for android graphics rendering ?

If any pxp support for android,please let me know.

Thanks & Regards,

Sankar.

Labels (3)
0 Kudos
Reply
4 Replies

2,327 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sankar

one can try to reuse patch provided on below link

qtbase: Enable support for i.MX SoCs with PXP · Freescale/meta-fsl-arm@9356268 · GitHub 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,327 Views
sankarsalla
Contributor II

Hi igor,

Thanks for your reply.

I thought that patch related to Qt,I need patch for android.

If android have any pxp support patch please share.

Thanks & Regards,
Sankar.

0 Kudos
Reply

2,327 Views
sankarsalla
Contributor II

Hi igor,

Can you please give some inputs,how to integrate Qt patch to android  which you suggest for pxp.

Actually i am working on pxp support for android, so if any pxp support available for imx7 android please share the inputs.

Thanks & Regards,

Sankar.   

0 Kudos
Reply

2,327 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sankar

in general bsp additional features can be added with help of  NXP Professional Services:

http://www.nxp.com/support/nxp-professional-services:PROFESSIONAL-SERVICE

Best regards
igor

0 Kudos
Reply