pulseaudio

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

pulseaudio

3,623件の閲覧回数
sunzhangyang
Contributor I

ShenweiWang‌

         我现在调试AP6212 的蓝牙,pulseaudio 一直运行不起来,

        [pulseaudio] main.c: Running in system mode, but --disallow-exit not set!
W: [pulseaudio] main.c: Running in system mode, but --disallow-module-loading not set!
N: [pulseaudio] main.c: Running in system mode, forcibly disabling SHM mode!
N: [pulseaudio] main.c: Running in system mode, forcibly disabling exit idle time!
W: [pulseaudio] main.c: Home directory of user 'pulse' is not '/home/pulse/output/var/run/pulse', ignoring.
W: [pulseaudio] caps.c: Normally all extra capabilities would be dropped now, but that's impossible because PulseAudio was built without capabilities support.
W: [pulseaudio] main.c: OK, so you are running PA in system mode. Please note that you most likely shouldn't be doing that.
W: [pulseaudio] main.c: If you do it nonetheless then it's your own fault if things don't work as expected.
W: [pulseaudio] main.c: Please read http://pulseaudio.org/wiki/WhatIsWrongWithSystemMode for an explanation why system mode is usually a bad idea.
W: [pulseaudio] random.c: Failed to get proper entropy. Falling back to unsecure pseudo RNG.
E: [pulseaudio] main.c: Sink input does not exist.
E: [pulseaudio] main.c: Source output does not exist.

pusleaudio 运行起来了但是运行pacmd 出现如下错误:

 [root@farsight bin]#pacmd
No PulseAudio daemon running, or not running as session daemon.

能帮忙看下是什么问题吗?

thanks

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

3,234件の閲覧回数
sunzhangyang
Contributor I

any answer?

0 件の賞賛
返信

3,234件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi Sun,

  

    Actually, Pulseaudio has been out of our support range, it is not relased by NXP.

    You can get experience from internet. see the link, please!

嵌入式linux开发板使用pulseaudio连接蓝牙耳机播放音频文件 - CSDN博客 

[Reminder] At first, you should ensure your Bluetooth is no problem!

Have a nice day!

TIC Weidong Sun

0 件の賞賛
返信