pull-up/pull-down resistors's tolerance

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

pull-up/pull-down resistors's tolerance

ソリューションへジャンプ
2,653件の閲覧回数
ko-hey
Senior Contributor II

Hi all

I have a question about resistance tolerance.

I want to know the resistance tolerance of GPIO's pull-up/pull-down resistors.

I can't find it in section 4.6.2 of following datasheet.

http://cache.nxp.com/files/32bit/doc/data_sheet/IMX6SDLIEC.pdf

Please provide the spec.

ko-hey

ラベル(1)
0 件の賞賛
返信
1 解決策
2,496件の閲覧回数
art
NXP Employee
NXP Employee

The tolerance of the i.MX6 series internal pull-up/down I/O resistors is +/- 10%.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,497件の閲覧回数
art
NXP Employee
NXP Employee

The tolerance of the i.MX6 series internal pull-up/down I/O resistors is +/- 10%.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,496件の閲覧回数
ko-hey
Senior Contributor II

Is the data described somewhere in RM ?

Ko-hey

0 件の賞賛
返信