pthread failed while bt call in imx8qm-mek

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

pthread failed while bt call in imx8qm-mek

1,909 Views
vinothkumars
Senior Contributor IV

Hi,

Board: IMX8QM-MEK

OS: Android 9 Automotive

 

How to resolve the following error from alsa layer,

pthread_create sched_setscheduler(1, {3}) call failed: Operation not permitted

pthread_create sched_setscheduler(1, {3}) call failed: Operation not permitted

 

//create rx task, use real time thread.
pthread_attr_init(&attr);
pthread_attr_setschedpolicy(&attr, SCHED_FIFO);
schParam.sched_priority = 3;
pthread_attr_setschedparam(&attr, &schParam);

adev->b_sco_rx_running = true;
ret = pthread_create(&tid_sco_rx, &attr, sco_rx_task, (void *)adev);
if(ret) {
goto error;
}
adev->tid_sco_rx = tid_sco_rx;
ALOGI("sco_rx_task create ret %d, tid_sco_rx %ld", ret, tid_sco_rx);

 

 

 

Regards,

Regards,
Vinothkumar Sekar
0 Kudos
Reply
1 Reply

1,890 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

 

It will depend if the BT module you are working with is supported on the BSP as mentioned in the following thread: https://community.nxp.com/t5/i-MX-Processors/Does-i-MX-8M-Nano-EVK-Bluetooth-module/m-p/1092753

 

BR,

Ivan.

0 Kudos
Reply