problem with imxcompositor-g2d

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

problem with imxcompositor-g2d

2,246件の閲覧回数
zohargolan
Contributor III

hello community,

i am using imx8mp and I am trying to display an overlay on top of a video. The overlay is sent to the buffer in appsrc. When my pipeline is just the video source -> queue1-> imxcompositor -> sink then I’m getting 60fps. I added appsrc to the pipeline in the form appsrc -> queue2 -> imxcompositor and the compositor goes to the same sink as the videoSrc flow. When I add appsrc to the pipeline but don’t push up a buffer to it with g_signal_emit_by_name(appsrc, "push-buffer", overlayBuffer, &ret), it drops to 30fps. When I start pushing buffers to the appsrc the framerate drops to 8 – 15 fps. The appsrc I’m using includes a format capability set to “BGRA”, I noticed that when I removed the capability, the framerate increased to 60fps but I’m unable to send data to the buffer in that scenario. The video source I’m using is v4l2src, the compositor is imxcompositor_g2d, and the sink is waylandsink.

For my application it is critical to maintain 60fpg video frame rate 

Any comment will be appreciated

Zohar

 

0 件の賞賛
返信
3 返答(返信)

2,184件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

I have already mailed to you, pls check it

0 件の賞賛
返信

1,699件の閲覧回数
Yannick31
Contributor I

Hello,

 

I have the same problem can we have the solution ?

 

Thanks 

0 件の賞賛
返信

1,686件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

pls create a new thread for your request, attach your detailed issue, you can submit here or click "submit a ticket" from the link as below, try to use company mail address to submit

Support | NXP Semiconductors

 

0 件の賞賛
返信