I want cross compile qt5.6 for imx6sx,but the lastest Qt version of yocto(i use imx-4.1.15-1.0.0_ga) is 5.5.1,
so i replace source/meta-qt5 with new meta-qt5 directory git clone from https://github.com/meta-qt5/meta-qt5.git and the branch is krogoth,then,bitbake fsl-image-qt5 without any problem except these warnings:
WARNING: QA Issue: gdb: invalid PACKAGECONFIG: readline [invalid-packageconfig]
WARNING: lttng-modules: no modules were created; this may be due to CONFIG_TRACEPOINTS not being enabled in your kernel.
WARNING: QA Issue: devil rdepends on tiff, but it isn't a build dependency? [build-deps]
WARNING: QA Issue: devil rdepends on liblzma, but it isn't a build dependency? [build-deps]
WARNING: QA Issue: The /usr/share/info/dir file is not meant to be shipped in a particular package. [infodir]
WARNING: QA Issue: qtbase-plugins rdepends on freetype, but it isn't a build dependency? [build-deps]
WARNING: QA Issue: qtbase-plugins rdepends on fontconfig, but it isn't a build dependency? [build-deps]
WARNING: QA Issue: qtbase rdepends on freetype, but it isn't a build dependency? [build-deps]
WARNING: QA Issue: qtbase rdepends on libicui18n, but it isn't a build dependency? [build-deps]
WARNING: QA Issue: qtbase rdepends on fontconfig, but it isn't a build dependency? [build-deps]
WARNING: QA Issue: qtbase rdepends on libicuuc, but it isn't a build dependency? [build-deps]
WARNING: QA Issue: imx-gpu-viv: /imx-gpu-viv-tools/usr/bin/gmem_info is owned by uid 1000, which is the same as the user running bitbake. This may be due to host contamination [host-user-contaminated]
WARNING: QA Issue: imx-gpu-viv: /imx-gpu-viv-tools-apitrace/usr/lib/apitrace/wrappers/egltrace.so is owned by uid 1000, which is the same as the user running bitbake. This may be due to host contamination [host-user-contaminated]
but when i burn u-boot,zImage and rootfs to imx6 and run the qt demo(qt5everywheredemo-1.0), Segmentation fault is display like this:
file:///usr/share/qt5everywheredemo-1.0/qml/QtDemo/main.qml:124:5: QML FontLoader: Cannot load font: "file:///usr/share/qt5everywheredemo-1.0/qml/QtDemo/fonts/PatrickHandSC-Regular.ttf"
Segmentation fault.
so i make a test, test.qml like this:
Rectangle{
color:"green";
}
it can run well; but when i add a line to Rectangle like this
Rectangle{
color:"green"
Text{text:"this is a test"}
}
I got a Segmentation fault again.
please tell me what should i do , thank you.
I have tried append freetype fontconfig uic these things to RDEPENDS and DEPENDS in source/meta-qt5/recipes-qt/qt5/qtbase_git.bb,but nothing changed.
解決済! 解決策の投稿を見る。
Hi Bio_TICFSL
Can you describe details about what should i do, how to configure qtbase and eglfs with yocto . Whether the approach that replace meta-qt5 layer with new meta-qt5 directory git clone from https://github.com/meta-qt5/meta-qt5.gitis feasible
Hi Chen,
Apparently you need configure qtbase and build with eglfs in order to work with Qt5.6, also check DEGL_API_FB=1 to prevent imx-gpu-viv from including Xlib from EG/vivante.h
Hope this helps
Hi Bio_TICFSL
Can you describe details about what should i do, how to configure qtbase and eglfs with yocto . Whether the approach that replace meta-qt5 layer with new meta-qt5 directory git clone from https://github.com/meta-qt5/meta-qt5.gitis feasible