prebuilt image for imx6qsabresd evaluation kit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

prebuilt image for imx6qsabresd evaluation kit

1,573件の閲覧回数
sachusanal
Contributor III

Hai  sir ,

could you please provide the link which i can download the prebuilt image of imx6qsabresd evaluation kit (which is provided by freescale when the board purchasing)

Board:IMX6QSABRESD Board

because  i need to test my sabresd board evaluation kit

please provide that one.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,419件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi sachu

demo images can be found on link below

L3.14.28_1.0.0_iMX6QDLS_BUNDLE  : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo Linux Binary Demo Files

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,419件の閲覧回数
sachusanal
Contributor III

Hai Igor ,

Thanks for your response.

let me know in that link where i can find the demo image. i couldn't seen anything there...

please help me

0 件の賞賛
返信