ppp not response for Audio Framework startup

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ppp not response for Audio Framework startup

2,676 次查看
run_zhao
Contributor I

   l try to start i.MX 8M Audio Framework  by docment ,named i.MX 8M Audio Framework Customer Post Processing SDK User’s Guide.

   step as below

 1,root@imx8mmevk:~# jinit.sh
Setting cpu cpufreq governor to performance
CPU running at 1800000 kHz
Loading jailhouse module

 2,root@imx8mmevk:/usr/local/bin# jstart.sh pp_sample
64+0 records in
64+0 records out
65536 bytes (66 kB, 64 KiB) copied, 0.000289375 s, 226 MB/s
1
Initializing Jailhouse hypervisor v0.9.1 (51-gc6c5e84) on CPU 2
Code location: 0x0000ffffc0200060
Page pool usage after early setup: mem 33/993, remap 64/131072
Initializing processors:
 CPU 2... OK
 CPU 1... OK
 CPU 3... OK
 CPU 0... OK
Initializing unit: irqchip
Initializing unit: ARM SMMU
No SMMU
Initializing unit: PCI
Adding virtual PCI device 00:00.0 to cell "imx8mm"
iommu_config_commit imx8mm
Page pool usage after late setup: mem 39/993, remap 336/131072
Activating hypervisor
1+1 records in
[ 1373.941354] OF: PCI: host bridge /pci@0 ranges:

11587 bytes (12 kB, 11 KiB) copi[ 1373.948067] OF: PCI:   MEM 0xbb900000..0xbb901fff -> 0xbb900000
ed, 0.000174375 s, 66.4 MB/s
com[ 1373.956890] pci-host-generic bb800000.pci: ECAM at [mem 0xbb800000-0xbb8fffff] for [bus 00]
mand line: [pp_sample]
startup f[ 1373.968179] pci-host-generic bb800000.pci: PCI host bridge to bus 0000:00
ile: [/usr/local/share/rest/defau[ 1373.977713] pci_bus 0000:00: root bus resource [bus 00]
lt.rest]
Enabling jailhouse root[ 1373.985773] pci_bus 0000:00: root bus resource [mem 0xbb900000-0xbb901fff]
 cell
[ 1373.995781] pci 0000:00:00.0: BAR 0: assigned [mem 0xbb900000-0xbb9000ff 64bit]
[ 1374.003747] virtio-pci 0000:00:00.0: enabling device (0000 -> 0002)
[ 1374.010432] ivshm 0000:00:00.0: name:register base: bb900000 size: 100
[ 1374.016978] ivshm 0000:00:00.0: name:shm base: bba00000 size: 200000
[ 1374.023586] ivshm_pipe_thread: entry
[ 1374.023609] ivshm_pipe_init:729: IRQ: 0xdb
[ 1374.023612] ivshm_pipe_init:730: IO Mapping: ffff000009c85000
[ 1374.023615] ivshm_pipe_init:731: SHM Mapping: [ffff000016a00000-ffff000016bfffff]
[ 1374.023616] ivshm_pipe_init:732: IVpos: 0
[ 1374.026051] The Jailhouse is opening.
[ 1375.064470] Initializing linux AF RPC services
[ 1375.069036] Cannot find rpcdev with endpoint id 256
[ 1375.074085] Cannot find rpcdev with endpoint id 257
Creating jailhouse lk cell
[ 1375.110711] CPU0: shutdown
[ 1375.113429] psci: CPU0 killed.
[ 1375.146665] CPU1: shutdown
[ 1375.149378] psci: CPU1 killed.
Adding virtual PCI device 00:00.0 to cell "lk"
Shared memory connection established: "lk" <--> "imx8mm"
iommu_config_commit lk
Created cell "lk"
Page pool usage after cell creation: mem 53/993, remap 336/131072
[ 1375.172139] Created Jailhouse cell "lk"
Loading jailhouse lk cell
Cell "lk" can be loaded
Starting lk cellStarted cell "lk"

waiting for sysfs entry [/sys/dev[ 1377.292411] ivshm_pipe_fsm:542: Initialization IVSHM services...
ices/platform/bb800000.pci/pci000[ 1377.300682] ivshm_endpoint_thread:259: buf rpmsg_ppp: [ffff800013740000-ffff800013741fff]
0:00/0000:00:00.0/0000:00:00.0.rp[ 1377.302169] ivshm_endpoint_thread:259: buf rpmsg_console: [ffff80001220a000-ffff80001220bfff]
msg_ppp.-1.-1/ppp]...
[ 1377.304184] ivshm_endpoint_thread:259: buf rpmsg_alsa: [ffff800013900000-ffff8000139fffff]
[ 1377.304256] ivshm_endpoint_thread:259: buf rpmsg_alsa: [ffff800017d84000-ffff800017d84fff]
[ 1377.304312] ivshm_endpoint_thread:259: buf rpmsg_alsa: [ffff800013b00000-ffff800013bfffff]
[ 1377.304526] ivshm_endpoint_thread:259: buf rpmsg_alsa: [ffff800017d01000-ffff800017d01fff]
[ 1377.305875] ivshm_endpoint_thread:259: buf cipc: [ffff800012208000-ffff800012209fff]
[ 1377.307604] ivshm_endpoint_thread:259: buf rpmsg-bin: [ffff800017982000-ffff800017983fff]
[ 1377.310044] ivshm_endpoint_thread:259: buf audio-weaver-rpmsg: [ffff8000176ac000-ffff8000176adfff]
[ 1377.311859] ivshm_endpoint_thread:259: buf rpmsg-wd: [ffff800012248000-ffff800012249fff]
[ 1377.313436] ivshm_endpoint_thread:259: buf lktraces: [ffff800013710000-ffff800013711fff]
[ 1377.316074] ivshm_endpoint_thread:259: buf rpmsg_rpc_hdmi: [ffff8000173fe000-ffff8000173fffff]
[ 1377.317298] ivshm_endpoint_thread:259: buf rpmsg_rpc_dac: [ffff8000173fa000-ffff8000173fbfff]
wait for pipeline... (1)
wait for pipeline... (2)
wait for pipeline... (3)
wait for pipeline... (4)
wait for pipeline... (5)
wait for pipeline... (6)
wait for pipeline... (7)
wait for pipeline... (8)
wait for pipeline... (9)
wait for pipeline... (10)
wait for pipeline... (11)
wait for pipeline... (12)
wait for pipeline... (13)
wait for pipeline... (14)
wait for pipeline... (15)
pipeline ready timeout
abort

device /sys/devices/platform/bb800000.pci/pci0000:00/0000:00:00.0/ppp is not ready.

in fact ,dectect node via "echo -n "PUT pipeline1/volume.elt/volume0/gain=0.6" > /sys/devices/platform/bb800000.pci/pci0000:00/0000:00:00.0/ppp" , but response always is ERROR.

how does l fix it ? thanks

标签 (1)
0 项奖励
回复
4 回复数

2,575 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Zhao,

Do you have connected the Audio board to the MX8MMini? this kinds of issues give you when you have not connected.

Regards

0 项奖励
回复

2,575 次查看
run_zhao
Contributor I

Hi,Bio

      l have confirmed that connect ribbon cable from J1001 of i.MX8MMini EVK board to J2500 of Audio board.

but audio board have not inserted DC powerd , not connect HDMI output of DVD/Blu-Ray player to HDMI RXC input port of Audio board.

     Is it necessary to supply power to audio board separately?

     thanks

   

20191030_091714.jpg

0 项奖励
回复

2,575 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Yes, you need power the Audio board

HDMI OUT to TV

HDMI RXC to blueray

Regards

0 项奖励
回复

2,575 次查看
run_zhao
Contributor I

Ok,Thanks for your support.

0 项奖励
回复