poweroff mx6 in u-boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

poweroff mx6 in u-boot

2,939 次查看
GregT
Contributor III

Does anyone know of a function in u-boot that can be called to power off the mx6 processor similar to the poweroff available in Linux?  Thanks.

标签 (2)
0 项奖励
回复
3 回复数

2,243 次查看
BiyongSUN
NXP Employee
NXP Employee

Set TOP field in SNVS_LP Control (LPCR), which will trigger i.MX6 PMIC_ON_REQ with the Dump PMIC enabled.

Untitled.png

2,243 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  If board hardware allows it - it is possible to use i.MX6 PMIC_ON_REQ signal

to switch off external PMIC.

 

How to control the PMIC_ON_REQ pin by SW without ON/OFF pin for i.MX6 

Regards,

Yuri.

2,243 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi GregT

For proper answer and discussion, Please check:

https://community.nxp.com/thread/307212 

Regards