Hi
We trying to use buffers queue for vpu encoder. We allocate several frame buffers and try to it to encoder in following way
enc_param.picStreamBufferAddr = output_mem_desc.phy_addr;
enc_param.picStreamBufferSize = output_mem_desc.size;
ret = vpu_EncStartOneFrame(handle, &enc_param);
.
.
.
ret = vpu_EncGetOutputInfo(handle, &outinfo);
But the buffer is not updated.
From following statement in docs
picStreamBufferAddr is a start address of a picture stream buffer under line-buffer mode and dynamic buffer allocation
I understand that while opening encoder instance i should set ringBufferEnable and dynamicAllocEnable as follows:
| encop.ringBufferEnable = 0; | |
| encop.dynamicAllocEnable = 1; |
But from the same doc file it appears
dynamicAllocEnable is not used in i.MX 6Dual/6Quad.
Deos it mean that there is no way to use several output buffers in encoder on i.MX 6Dual/6Quad, ?
Maybe there is some other set of flags we should set ?
Thanks.
refer to your information, you can use the ring-buffer mode,
When using a ring-buffer scheme with a limited size of encoder stream buffer, stream reading during encoder operation is recommended. Using two dedicated functions, vpu_EncGetBitStreamBuffer() and vpu_EncUpdateBitStreamBuffer(), the application can easily handle the read pointer while accessing the encoder bitstream buffer.