phy link never came up issue ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

phy link never came up issue ?

4,167 次查看
peteramond
Contributor V

Dear All,

My hardware is based on iMAX6Q processor and the design most similar to nitrogen6_max development board. 

I'm using Boundary devices u-booot version 2016.03 and linux kernel - Linux-boundary 4.1.15.

I am trying to interface PCIE with TW6865 Intersil video chip

I did following latest hardware change to PCIE clk differential pair as NXP explained in their hardware guide lines.

pastedImage_2.png

But I'm getting following error while kernel loading. And PCIE is not working.

imx6q-pcie 1ffc000.pcie: phy link never came up
imx6q-pcie 1ffc000.pcie: Link never came up
imx6q-pcie 1ffc000.pcie: failed to initialize host
imx6q-pcie: probe of 1ffc000.pcie failed with error -110

Could you please give me a solution for this.

Regards.

Peter.

标签 (4)
0 项奖励
回复
1 回复

3,999 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Peter

boundary software issues are often resolved by upgrading uboot

https://boundarydevices.com/how-to-upgrade-u-boot/ 

For "phy link never came up issue" one can check suggestions on:

pcie "phy link never came up" on sabresd running dora 3.10.17_beta 

iMX6q PCIe phy link never came up on kernel v4.4.x - Patchwork 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复