pfuze100 IRQ handler missing?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

pfuze100 IRQ handler missing?

2,591件の閲覧回数
jaiminthakkar
Contributor II

I was going through "drivers/regulator/pfuze100-regulator.c" and I noticed that driver doesn't have IRQ handler.

But interrupt line of PMIC PFUZE100 is connected to IMX6 on SABRE board.

Is IRQ handler is missing in driver or It is not required?

If it is not required then why interrupt line of PMIC is connected to IMX6 in SABRE?

ラベル(4)
0 件の賞賛
返信
3 返答(返信)

2,192件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi,

For the following answer, I’m assuming that you are referring to the INTB pin of the PMIC, please correct me if I’m wrong.

INTB is an open drain, active low output. It is asserted when any fault occurs, provided the fault interrupt is unmasked. INTB is de-asserted after the fault interrupt is cleared by software, which requires writing a “1” to the fault interrupt bit.

You can find the interrupt handling and interrupt bit summary in section 6.5.3 and section 6.5.4 of the MMPF0100 datasheet: http://cache.nxp.com/files/analog/doc/data_sheet/MMPF0100.pdf


Have a great day,
Jose Reyes

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,192件の閲覧回数
mukelarvin
Contributor IV

Have the interrupts been implemented in a newer version of the driver or is that still up to us at this point?

0 件の賞賛
返信

2,192件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi Luke,

I’m afraid not, the interrupts have not been implemented in the PFUZE driver.


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信