Hi,
I upgrade my Linux kernel from 5.15.52 to 6.6. After upgrading my panel only shows a small stripe. I made no changes at the device tree. When I use the panel-simple driver instead of panel-lvds I got a working display. Does someone know about changes in the driver.
I use a iMX8MP and my panel is connected to LVDS1 interface.
dmesg shows a message but I can't identify the failure
dmesg | grep lvds
[ 0.077630] platform panel-lvds1: Fixed dependency cycle(s) with /ldb-display-controller/lvds-channel@1
[ 2.511277] imx8mp-ldb ldb-display-controller: Failed to create device link (0x180) with phy-lvds
[ 2.552129] imx8mp-ldb ldb-display-controller: Failed to create device link (0x180) with panel-lvds1
Thanks
Hello,
Have you checked the dtb? are they changed? which lvds device are you working on?
Regards
Here are my settings. Maybe you find a mistake
/ {
backlight1: backlight1 {
compatible = "pwm-backlight";
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_lvds1>;
default-brightness-level = <6>;
pwms = <&pwm3 0 50000 0>;
power-supply = <®_lvds1_reg_en>;
enable-gpios = <&gpio2 20 GPIO_ACTIVE_LOW>;
brightness-levels= <0 4 8 16 32 64 128 255>;
status = "okay";
};
panel_lvds: panel-lvds1 {
compatible = "panel-lvds";
backlight = <&backlight1>;
width-mm = <218>;
height-mm = <137>;
data-mapping = "vesa-24";
status = "okay";
panel-timing {
clock-frequency = <71000000>;
hactive = <1280>;
hfront-porch = <30>;
hsync-len = <48>;
hback-porch = <80>;
vactive = <800>;
vfront-porch = <3>;
vsync-len = <6>;
vback-porch = <14>;
};
port {
panel1_in: endpoint {
remote-endpoint = <&lvds1_out>;
};
};
};
};
&lcdif2 {
status = "okay";
};
/* LVDS1 */
&ldb {
status = "okay";
lvds-channel@1 {
#address-cells = <1>;
#size-cells = <0>;
status = "okay";
primary;
port@1 {
reg = <1>;
lvds1_out: endpoint {
remote-endpoint = <&panel1_in>;
};
};
};
};
&ldb_phy {
status = "okay";
};