ogg support with aiurdemux

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ogg support with aiurdemux

1,210 次查看
dabrain
Contributor I

dear all,

I'm using yocto dora branch from meta-fsl-arm and 'im facing an issue with ogg demux. Indeed gstreamer-0.10 uses aiurdemux to handle ogg file and i'm facing an error.

0:00:00.135230334  1160    0x80460 WARN               aiurdemux

aiurdemux.c:3756:aiurdemux_loop_state_header: Warning:

API[initializeIndex] not implement!

0:00:00.135399334  1160    0x80460 WARN               aiurdemux

aiurdemux.c:3448:aiurdemux_set_readmode: API[setReadMode] failed, ret=-6

0:00:00.135473334  1160    0x80460 ERROR              aiurdemux

aiurdemux.c:3469:aiurdemux_set_readmode: ***final file mode

0:00:00.135534000  1160    0x80460 WARN               aiurdemux

aiurdemux.c:3767:aiurdemux_loop_state_header: Warning:

API[getNumPrograms] not implement!

And then vorbidec fails to decode audio packet.

When i disable ogg support in /usr/share/aiur_registry_arm11.cf and so gstreamer is using oggdemux element, the file is correctly decoded.

Is there some fixes concerning this parser ? Is there acceleration in aiur demux ?

Best regards.

Stéphane

标签 (4)
0 项奖励
回复
1 回复

852 次查看
LeonardoSandova
Specialist I

Hi

On latest Freescale Yocto release (3.10.17), there were several changes on freescale's gstreamer elements in order to be "friendlier" with the rest of the open source elements, so it may be the case that latest code has fixed this issue. Not sure when the metadata migration will finish (from 3.10.17 to community master) so for the moment you can try removing it or lowering its rank.

Leo

0 项奖励
回复