number of TPM (timer PWM module) channels in imx8qxp

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

number of TPM (timer PWM module) channels in imx8qxp

1,173件の閲覧回数
dsp4us
Contributor I

 i.MX 8DualX/8DualXPlus/8QuadXPlus Applications Processor Reference Manual (chapter 12.7) states

The TPM (Timer/PWM Module) is a 2- to 8-channel timer which supports input capture,
output compare, and the generation of PWM signals to control electric motor and power
management applications.

on other hand in list of the features (chapter 1.1.2) in the same document

1x TPM (Timer PWM Module) with 2 channels

that could be confirmed by looking at pinout of imx8qxp chip (as example)

#cortex_m4

Could someone point me to the processor model that has more TPM available channels? Might be from different families of imx8? In upcoming design we need 6 independent free running timer capturing channels.

Thanks.

0 件の賞賛
返信
1 返信

1,131件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Michael,

The i.MX8QXP has 1 TPM timer with 2 channels, you have about 4 PWM managed by FlexTimer module.

Regards

0 件の賞賛
返信