nativesdk-u-boot-imx-tools-2022.04-r0 do_fetch

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

nativesdk-u-boot-imx-tools-2022.04-r0 do_fetch

217 次查看
rprronad
Contributor IV

Dear Experts

I'm working on the yocto-project (kirkstone release) with custom board based on imx6ull processor and while generating the the sdk for the image i got the below fetch error :

ERROR: nativesdk-u-boot-imx-tools-2022.04-r0 do_fetch: Fetcher failure: Fetch command export PSEUDO_DISABLED=1; export DBUS_SESSION_BUS_ADDRESS="unix:path=/run/user/1000/bus"; export SSH_AUTH_SOCK="/run/user/1000/keyring/ssh"; export PATH="/home/calixto-systems/Desktop/calixto-yocto-bsp/sources/poky/scripts/nativesdk-intercept:/home/calixto-systems/Desktop/calixto-yocto-bsp/build/tmp/sysroots-uninative/x86_64-linux/usr/bin:/home/calixto-systems/Desktop/calixto-yocto-bsp/build/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-u-boot-imx-tools/2022.04-r0/recipe-sysroot-native/usr/bin/chrpath-native:/home/calixto-systems/Desktop/calixto-yocto-bsp/sources/poky/scripts:/home/calixto-systems/Desktop/calixto-yocto-bsp/build/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-u-boot-imx-tools/2022.04-r0/recipe-sysroot-native/usr/bin/x86_64-pokysdk-linux:/home/calixto-systems/Desktop/calixto-yocto-bsp/build/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-u-boot-imx-tools/2022.04-r0/recipe-sysroot/usr/local/oe-sdk-hardcoded-buildpath/sysroots/x86_64-pokysdk-linux/usr/bin/crossscripts:/home/calixto-systems/Desktop/calixto-yocto-bsp/build/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-u-boot-imx-tools/2022.04-r0/recipe-sysroot-native/usr/sbin:/home/calixto-systems/Desktop/calixto-yocto-bsp/build/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-u-boot-imx-tools/2022.04-r0/recipe-sysroot-native/usr/bin:/home/calixto-systems/Desktop/calixto-yocto-bsp/build/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-u-boot-imx-tools/2022.04-r0/recipe-sysroot-native/sbin:/home/calixto-systems/Desktop/calixto-yocto-bsp/build/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-u-boot-imx-tools/2022.04-r0/recipe-sysroot-native/bin:/home/calixto-systems/Desktop/calixto-yocto-bsp/sources/poky/bitbake/bin:/home/calixto-systems/Desktop/calixto-yocto-bsp/build/tmp/hosttools"; export HOME="/home/calixto-systems"; LANG=C git -c core.fsyncobjectfiles=0 -c gc.autoDetach=false -c core.pager=cat clone --bare --mirror https://github.com/nxp-imx/uboot-imx.git /home/calixto-systems/Desktop/calixto-yocto-bsp/downloads//git2/github.com.nxp-imx.uboot-imx.git --progress failed with exit code 128, no output

ERROR: nativesdk-u-boot-imx-tools-2022.04-r0 do_fetch: Bitbake Fetcher Error: FetchError('Unable to fetch URL from any source.', 'git://github.com/nxp-imx/uboot-imx.git;protocol=https;branch=lf_v2022.04')

ERROR: Logfile of failure stored in: /home/calixto-systems/Desktop/calixto-yocto-bsp/build/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-u-boot-imx-tools/2022.04-r0/temp/log.do_fetch.4159

ERROR: Task (virtual:nativesdk:/home/calixto-systems/Desktop/calixto-yocto-bsp/sources/meta-imx/meta-bsp/recipes-bsp/u-boot/u-boot-imx-tools_2022.04.bb:do_fetch) failed with exit code '1'


Please someone can help out for this error.

Thanks and Regards,

Ravikumar

0 项奖励
回复
1 回复

203 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Have you followed our IMX_YOCTO_PROJECT_USERS_GUIDE document?

0 项奖励
回复