nand booting problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

nand booting problem

1,741 Views
PramodKumar
Contributor IV

hii

when i m loading the imx23_linux.sb  image in nand on imx233 board using kobs-ng its producing this type of error plz tell me how to solve

root@freescale /mmc$ kobs-ng init imx23_linux.sb

rom_version:0x0

nand_erase_nand: attempt to erase a bad block at page 0x00000000

mtd: device 0 fanand_erase_nand: attempt to erase a bad block at page 0x00000040

ils MEMERASE (0xnand_erase_nand: attempt to erase a bad block at page 0x00000080

0 - 0x40000)

mtd: Failenand_erase_nand: attempt to erase a bad block at page 0x000000c0

d to erase block @0x0

mtd: device 0 fails MEMERASE (0x40000 - 0x40000)

mtd: Failed to erase block @0x40000

mtd: device 0 fails MEMERASE (0x80000 - 0x40000)

mtd: Failed to erase block @0x80000

mtd: device 0 fails MEMERASE (0xc0000 - 0x40000)

mtd: Failed to erase block @0xc0000

Original Attachment has been moved to: booting_kernel.txt.zip

Labels (4)
0 Kudos
Reply
1 Reply

1,313 Views
igorpadykov
NXP Employee
NXP Employee

Hi Pramod

one can try attached NAND erase tool, its purpose to return NAND

flash that was programmed with the Linux BSP back to the factory settings.

Also one can try more new kobs-ng tool

Index of /buildsources/k/kobs-ng/kobs-ng-3.0.35-4.0.0

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply