mx53 cspi clk source

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mx53 cspi clk source

1,733 Views
pensive
Fresh Out Contributor

how to use Low-Frequency Reference Clock for cspi . CSPI_PERIODREG=0x8000 is not

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,667 Views
igorpadykov
NXP Employee
NXP Employee

Hi peng

CSPI_PERIODREG is used for clock defining pause beteween data transfers.

CSPI data transfer clocks are defined using ECSPIx_CONREG dividers

and CCM ECSPI_CLK_ROOT, check Figure 18-2. CCM Clock Tree

i.MX53 Reference Manual (rev.2.1  6/2012)

http://www.freescale.com/files/32bit/doc/ref_manual/iMX53RM.pdf

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------