mx53 can‘t boot wince7 from SD Card

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mx53 can‘t boot wince7 from SD Card

ソリューションへジャンプ
2,949件の閲覧回数
JackyHuang
Contributor II

Dear All:

Im a newer in wince7.

Now my company design a mx53 board base on the mx53smd reference board. 

We just reduce the ddr from 1G to 512M!

we can't boot the wince7 from SD Card, there is no print output to the UART.

however, we can boot android from SD Card succeed.

so, what can I do to make the wince7 boot from SD Card succeed?

Thanks advance!

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
2,703件の閲覧回数
king_jin
NXP Employee
NXP Employee

You need to configure the correct parameters for DDR memory in bootloader(hardware should help). Next you should define the IMGRAM512 macro in BSP manually.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,703件の閲覧回数
liaoaleon
Contributor I

I had the same problem,Can anyone tell me have configure it?!

0 件の賞賛
返信
2,703件の閲覧回数
JackyHuang
Contributor II

Thanks for your help,  I'll try it

0 件の賞賛
返信
2,704件の閲覧回数
king_jin
NXP Employee
NXP Employee

You need to configure the correct parameters for DDR memory in bootloader(hardware should help). Next you should define the IMGRAM512 macro in BSP manually.

0 件の賞賛
返信