HIiiiiiiiii
I am working on mx53 QSB. I want to download the demo image file in micro SD card. For this purpose I download L2.6.35_11.09.01_ER_images_mx5x.tar but can not find the document how to load this demo image file in micro SD card. Please give me a procedure to load this file in micro SD card.
Second point is that I want to create our own image file, for this purpose I install LTIB and follow the procedure given in mx53 start linux bsp user guide upto 2.2.
But after that I can't understand what is the next procedure to create image file and load in micro SD card. On my host PC OS is ubuntu 10.04(32 bit).
Thank you
swapneel
1.
Please use the MFG tool to deploy the image(s).
Use section 5 (Downloading Images Using MFG Tool) of "i.MX53_START_Linux_BSP_UserGuide.pdf".
2.
Please use section 7 (Using a Linux Host to Set Up an SD/MMC Card) of "i.MX53_START_Linux_BSP_UserGuide.pdf".
Hiii
The other member of freescale community said that the MFG tool works only on windows. Is this correct? Then how to load the demo image file(L2.6.35_11.09.01_ER_images_mx5x.) to micro SD card on linux.?Please give me a step by step procedure to load this file.
2. For second point can I jump directly section 7 after 2.2 ?Is any step in between these is needed to
create our own image file?
Dear sir,
I install LTIB .As per the mx53 start linux bsp user guide.pdf in
step 2.2 upto step install one package to rootfs
(./ltib -m scdeploy -p u-boot) done successfully.
After that I go to section 7 using a linux host to set up an
microSD card. complete all the steps (screen shots are attached
here).
Then go to step 8.2 Run the image from MMC/SD. In that I connect vga
display to QSB. Connect serial port to my windows PC and configure it
to 115200-8-N-1 . press "POWER " key to power up the board but it
does not show any thing on VGA display as well as on hyperterminal.
Please check the attachment and guide me what is the problem
Thank you
swapneel
Thanks & Regards
swapneel
HIiiii
I follow all the commands in section 7 please see all 3 attachments..........
Please pay attention, the U-boot can be provided in two options :
with and without padding.
Please look at section 2.5 (How to generate no-padding U-Boot) of
i.MX53_START_Linux_BSP_UserGuide.pdf
To generate no-padding U-Boot, run:
sudo dd if=u-boot.bin of=u-boot-mx53-loco-no-padding.bin bs=512 skip=2
U-boot with padding contains two 512-blocks zone at the beginning.
When such U-boot is written to SD, using command dd, SD partition table will
be destroyed. But after writing U-boot and kernel via the dd command, it is
recommended to create new partition on the SD again, assuming, that the first
blocks, which contains U-boot and kernel must not be overlapped by the
partition. Therefore partition should be created skipping U-boot and kernel
zone. The partition information will be located in the first block of SD this
block does not cover U-boot significant information.
From section 6.3 (Use i.MX53 as Host Server to Create rootfs) :
the rootfs partition should be located after kernel image; the first 0x800000
bytes can be reserved for MBR, bootloader, and kernel sections.
Dear sir,
I generate no-padding U-Boot by using given command and use this
no padding u-boot-mx53-loco-no-padding.bin file to copying the boot
loader image and copying the kernal image. follow all command given in
section 7 of mx53 start linux bsp user guide.pdf.
After that insert the microSD card in mx53 QSB ,connect serial port
and configure it to 115200-8-N-1. connect VGA monitor to QSB.
connect power supply and press POWER switch so blue led on. but It
does not show any thing on hyper terminal also on VGA display. I
given command BBG U-Boot > printenv given in DOC-1554 but it does not
get this command.
I attach my complete procedure which i done in command promt from
start to end. Please check screenshot1 then screenshot2 and then
screenshot3. Is any thing is wrong in that ?
procedure:
1) Install LTIB on ubuntu 1004 upto step 2.2 at the point 8(
Install one package to rootfs)in mx53 start linux bsp user guide.pdf.
1) insert microSD card in card reader and connect the reader to
ubuntu pc.
2)open command promt and follow all instructions which are given in
section 7(please see screen shot1,2 and 3.)
3)After that insert the microSD card in mx53 QSB ,connect serial
port and configure it to 115200-8-N-1. connect VGA monitor to QSB.
connect power supply and press POWER switch so blue led on. but It
does not show any thing on hyper terminal also on VGA display. I
given command BBG U-Boot > printenv given in DOC-1554 but it does not
get this command.
Please guide me if any thing is wrong in this procedure or in
command.
Thanks & Regards
swapneel
HI
so After 2.2 i want to follow section 2.5 for no padding u-boot.
2) Then follow all the steps in section 6.3
3) Then go to all the steps in section 7 or any step in section 7 is drop?.
Is This correct?
please give me If you have any step by step information .