Procedure to load pre build image to micro SD card

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Procedure to load pre build image to micro SD card

1,616 次查看
swapneelsangar
Contributor II

HIiiiii

I am working on Mx53 QSB. I install LTIB on my host pc (ubuntu 10.04). Now I want to load pre build demo image file to micro SD card. So please give me a

procedure to load the prebuild image file to micro SD card.

Thank you.

swapneel

标签 (2)
0 项奖励
回复
3 回复数

1,365 次查看
swapneelsangar
Contributor II

Hiiiiii

I have some confusion about to load the file in micro SD card. means suppose I change splash then is there any compilation is needed? and how to load this file in micro SD card?? 

And which tool is used to load the file to microSD card in linux. Please give me a detail procedure about that tool.

Thank you

swapneel

0 项奖励
回复

1,365 次查看
LeonardoSandova
Specialist I

You need to use the manufacturing tool, download the documentation and check the corresponding section on the user guide. BTW, the MFG tool works only on windows. In case you want to flash under Linux, other tools are used.

Leo

0 项奖励
回复

1,365 次查看
swapneelsangar
Contributor II

Dear sir,

I install LTIB .As per the mx53 start linux bsp user guide.pdf in

step 2.2 upto step install one package to rootfs 

(./ltib -m scdeploy -p u-boot) done successfully.

After that I go to section 7  using a linux host to set up an

microSD card. complete all the steps (screen shots are attached

here).

Then go to step 8.2 Run the image from MMC/SD. In that I connect vga

display to QSB. Connect serial port to my windows PC and configure it

to 115200-8-N-1 . press "POWER " key to power up the board but it

does not show any thing on VGA display as well as on hyperterminal.

Please check the attachment and guide me what is the problem

Thank you

swapneel

 

0 项奖励
回复