Hi,all
I have install LTIB,and compile ok.
there is imx28_ivt_uboot.sb and imx28_ivt_linux.sb in the /opt/i.mx28x/L2.6.35_1.1.0_130130_source/source/ltib/rootfs/boot/
I can find linux-2.6.35 sourcecode in the /opt/i.mx28x/L2.6.35_1.1.0_130130_source/source/ltib/rpm/BUILD.
I can find imx-bootlets-src-2.6.35.3-1.1.0 sourcecode in the /opt/i.mx28x/L2.6.35_1.1.0_130130_source/source/ltib/rpm/BUILD.
I need to modify some uboot sourcecode,but where is uboot sourcecode??
thanks!!
已解决! 转到解答。
I´ve been using u-boot from Freescale/u-boot-fslc · GitHub, branch name patches-2014.01, but this u-boot does not need bootlets, if it´s a requirement for you it will not work.
In case you want to "taste" this u-boot, you can download this pre-built image:
from
it´s a framebuffer image. You can copy it to a sdcard using:
$ sudo dd if=fsl-image-machine-test-imx28evk-20140523-12.rootfs.sdcard of=/dev/sdX
Hi 浩华,
As Jimse has told you that use the commend:./ltib -m prep -p u-boot under ltib directory, you will find the source code.
Have a great day,
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------