mp4 decoder parse failed on i.mx6q SdabeSD linux OS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

mp4 decoder parse failed on i.mx6q SdabeSD linux OS

跳至解决方案
2,096 次查看
andypeng
Contributor I

Hi all,

  I test shwj.mp4 file run./ unit_tests/autorun-vpu.sh,hint follow information:

Running test case: ./mxc_vpu_test.out -C config_dec

[INFO]  VPU test program built on Mar 27 2013 20:44:36

[INFO]  Product Info: i.MX6Q/D/S

[INFO]  VPU firmware version: 2.1.8_r34588

[INFO]  VPU library version: 5.4.10

[INFO]  Format: STD_MPEG4

[INFO]  MPEG4 class: MPEG4

[INFO]  Input file "shwj.mp4" opened.

[INFO]  bitstreamMode 0, chromaInterleave 0, mapType 0, tiled2LinearEnable 0

[ERR]  vpu_DecGetInitialInfo failed, ret:-1, errorcode:-2147483648

[ERR]  decoder parse failed

autorun-vpu.sh: FAIL test case: ./mxc_vpu_test.out -C config_dec

autorun-vpu.sh: Exiting FAIL

Why? How coud I do?

Can anybody answer this question ?


NOTE:

    shwj.mp4 is about 7.2Mb.

0 项奖励
回复
1 解答
1,798 次查看
fabio_estevam
NXP Employee
NXP Employee

Please try to decode the file via a Gstreamer pipeline.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,798 次查看
fabio_estevam
NXP Employee
NXP Employee

Please try to decode the file via a Gstreamer pipeline.

0 项奖励
回复