modify Clock in Devicetree

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

modify Clock in Devicetree

1,358 次查看
himanshugusain
Contributor III

Hi

I am using the 3.10.53 kernel

the ipg_clock for fec driver i am getting is 66Mhz ,i want to modify

it to 50 Mhz

What change need to be done for that in devicetree ?

Regards

Himanshu

标签 (3)
0 项奖励
回复
1 回复

1,287 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Himanshu

ipg_clock is produced from AHB_CLK_ROOT as shown on

Figure 18-5. BUS clock generation http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

so changes in devicetree are not sufficient. It is necessary to reprogram pll2/3, producing

this clock.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复