mmcblk1: error -110 transferring data

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mmcblk1: error -110 transferring data

ソリューションへジャンプ
28,268件の閲覧回数
pfsang
Contributor IV

hi, all

        i encountered a problem about SD card.

        when i insert a SD card,  the following error log in console.

-----------------------------------------------------------------------------------

mmc1: new high speed SDHC card at address e624

mmcblk1: mmc1:e624 SU08G 7.40 GiB

root@freescale ~$

root@freescale ~$ mmcblk1: error -110 transferring data, sector 0, nr 8, cmd response 0x900, card status 0xb00

mmcblk1: retrying using single block read

mmcblk1: error -110 transferring data, sector 0, nr 8, cmd response 0x900, card status 0x0

end_request: I/O error, dev mmcblk1, sector 0

mmcblk1: error -110 transferring data, sector 1, nr 7, cmd response 0x900, card status 0x0

end_request: I/O error, dev mmcblk1, sector 1

------------------------------------------------------------------------------------

my iomux setting is here:

//USDHC2

MX6DL_PAD_SD2_CLK__USDHC2_CLK,

MX6DL_PAD_SD2_CMD__USDHC2_CMD,

MX6DL_PAD_SD2_DAT0__USDHC2_DAT0,

MX6DL_PAD_SD2_DAT1__USDHC2_DAT1,

MX6DL_PAD_SD2_DAT2__USDHC2_DAT2,

MX6DL_PAD_SD2_DAT3__USDHC2_DAT3,

//SD2_CD

MX6DL_PAD_GPIO_4__GPIO_1_4,

//SD2_WP

MX6DL_PAD_GPIO_2__GPIO_1_2,

------------------------------------------------------------------

sd2_data  is here:

#define AUTO_SD2_CD IMX_GPIO_NR(1, 4)

#define AUTO_SD2_WP IMX_GPIO_NR(1, 2)

static const struct esdhc_platform_data mx6q_sd2_data __initconst = {

  .cd_gpio = AUTO_SD2_CD,

  .wp_gpio = AUTO_SD2_WP,

  .keep_power_at_suspend = 1,

  .support_8bit = 0,

  .delay_line = 0,

  .cd_type = ESDHC_CD_CONTROLLER,

  .runtime_pm = 1,

};

ラベル(6)
0 件の賞賛
返信
1 解決策
18,131件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi fang,

simply put, your card outputs data

so fast, that OS just can not able to receive them.

Suggest to try more slower grade cards or

test old SD2.0 2GB SD card just for test.

Best regards

chip

元の投稿で解決策を見る

0 件の賞賛
返信
17 返答(返信)
18,131件の閲覧回数
zhaotao
Contributor I

hi,have you ever solved the problem? I have the same trouble,

can any help me?

Freeing unused kernel memory: 388K (809d7000 - 80a38000)
mmc3: Timeout waiting for hardware interrupt.
mmcblk3: error -110 transferring data, sector 7996552, nr 32, cmd response 0x900, card status 0xb00
mmcblk3: retrying using single block read
mmc3: Timeout waiting for hardware interrupt.
mmcblk3: error -110 transferring data, sector 12194864, nr 216, cmd response 0x900, card status 0xb00
mmcblk3: retrying using single block read

0 件の賞賛
返信
18,131件の閲覧回数
angelos
Contributor II

Hi all,

I've the same problem using a custom board with iMX6Solo.

The same HW works fine with kernel 3.0.35 but after switching to 3.10.17 I'm facing this issue.

* on 3.0.35 I have:

#define SD1_CD IMX_GPIO_NR(1, 1)

#define SD1_WP IMX_GPIO_NR(1, 9)

static const struct esdhc_platform_data mx6q_sd1_data __initconst = {

  .cd_gpio = SD1_CD,

  .wp_gpio = SD1_WP,

  .keep_power_at_suspend = 1,

  .support_8bit = 1,

  .delay_line = 0,

  .platform_pad_change = plt_sd3_pad_change,

  //.cd_type = ESDHC_CD_CONTROLLER,

};

On 3.10.17 I should apply the same settings through the dts file.

Do you know how should I set cd-gpios and wp-gpios?

&usdhc1 {

  pinctrl-names = "default";

  pinctrl-0 = <&pinctrl_usdhc1_1>;

  fsl,delay-line;

  fsl,cd-controller;

cd-gpios = <&gpio1 1 1>;        

/* cd-inverted;*/

wp-gpios = <&gpio1 9 1>;

/* max-frequency = <50000000>;*/

  keep-power-in-suspend;

// enable-sdio-wakeup;

// cap-sd-highspeed;

//    no-1-8-v;

  status = "okay";

};

Thanks in advance.

0 件の賞賛
返信
18,131件の閲覧回数
Igor
Contributor III

Hello Angelo,

Did you solve that problem?

I encountered your same issue: my eMMC memory no longer works properly switching from kernel 3.0.35 to 3.10.17 (or 3.10.53).

Thanks in advance.

0 件の賞賛
返信
18,131件の閲覧回数
angelos
Contributor II

Hello Igor,

in my case, the problem was strictly related to an external SD card.

BTW, it was not a SW problem - in fact, I found that with some SD card devices the issue was not reproducible.

Regards,

Angelo

0 件の賞賛
返信
18,131件の閲覧回数
Igor
Contributor III

Hello Angelo,

Thanks a lot for your fast reply.

Yesterday I received a new firmware release for that eMMC/SD: now it works properly with both new Linux Kernel Versions!

Regards,

Igor

0 件の賞賛
返信
18,131件の閲覧回数
Raana
Contributor III

Hi Igor,

I'm also facing the same kind of problem on my eMMC.

Platform detail: i.Mx6 SabreSD based custom board

Kernel: L3.0.35

Issue is, mmcblk2: error -110 sending stop command, original cmd response 0x900, card status 0x400e00

Screenshot from 2016-08-23 13-28-01.png

It's stopped after the issue (console also not alive)

What may be the issue ?

At the same time,

Where will get that latest firmware ? and How to update that (procedure or document)?

Thanks in Advance

Regards,

J.P.Raja

0 件の賞賛
返信
18,131件の閲覧回数
pfsang
Contributor IV

SD2_DAT0 and SD2_DAT1 just can  work.


i will create new thread for uSDHC 1bit mode configuration

0 件の賞賛
返信
18,131件の閲覧回数
pfsang
Contributor IV

hi, chipexpert

   but my sd card is  SD2.0 8G and is ok on sarbresd

0 件の賞賛
返信
18,131件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi fang,

suggest to test SD2 hardware with bare metal SD read/write test

"MX6_PLATFORM_SDK "

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&nodeId=018rH3ZrDRB24A&fpsp=1&t...

You can run it with jtag.

Best regards

chip

0 件の賞賛
返信
18,131件の閲覧回数
pfsang
Contributor IV

hi, chipexpert

       i have found the problem which is hardware issue.

       SD2_DAT0 and SD2_DAT1 can work.

       so how do i set the mode to 1bit mode?

0 件の賞賛
返信
18,131件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Sorry fang

do you mean

"SD2_DAT0 and SD2_DAT1 can NOT work." ?

For uSDHC 1bit mode configuration,

I think you should create new thread, since this is new

problem.

Best regards

chip

18,131件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi fang,

please look below thread with similar SD errors,

seems changing card solved problem

Boot problem: MCIMX6Q-SDB

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
18,131件の閲覧回数
pfsang
Contributor IV

hi, chipexpert

     i have tried to change three cards, but the problem still is not solved.

0 件の賞賛
返信
18,131件の閲覧回数
JackyAtFreescal
Senior Contributor II

Hi fang,

Could you try another SD port?

The problem may be came from the SD port socket.

Regards,

Jacky

18,131件の閲覧回数
pfsang
Contributor IV

hi, Jacky

   we have only one sd slot  on our board.

   how to  the SD port socket ?

B&R

0 件の賞賛
返信
18,132件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi fang,

simply put, your card outputs data

so fast, that OS just can not able to receive them.

Suggest to try more slower grade cards or

test old SD2.0 2GB SD card just for test.

Best regards

chip

0 件の賞賛
返信
18,131件の閲覧回数
YixingKong
Senior Contributor IV

JackyAtFreescale, could you please look after this SD card issue?

Thanks,

Yixing

0 件の賞賛
返信