mmc1: Timeout waiting for hardware interrupt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mmc1: Timeout waiting for hardware interrupt

4,851件の閲覧回数
lvguangzhao
Contributor I

Our product develop is base on I.MX6 SOLOLITE+ BSP L3.0.35_4.1.0, I have a wifi module bcm43241, connect to slot sd2, sdio sometimes occur "mmc1:Timeout waiting for hardware interrupt" when in process of "mmc_add_host", reboot 100 times happen about 2 times,After track mmc driver, we found that there is no irq generate when host prepare sending command, we have tried cut down the sdio interface in wifi module side, problem still happen, only adjust the boot sequence of sdio and mipi lcm can fix this issue, which means let sdio init first , lcm init later, So anyone can help explain why?

pastedImage_1.png

0 件の賞賛
返信
1 返信

3,150件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi lv

bcm43241 is not supported on official L3.0.35_4.1.0, may be recommended to apply

to vendor support for updated driver for that kernel version.

http://wireless.murata.com/eng/products/rf-modules-1/wi-fi-bluetooth-for-freescale-i-mx.html

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信